2019-08-15 10:26 AM
Good afternoon, I was trying to debug a program on my new stm32f103C8T6 chip using the st-link v2 programmer, but i always get the same error : Error: failed to erase memory
I have tried the procedure with multiple boards so i guess that the problem is software, here is the full console output :
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_k3pQvR.log
ST-LINK SN : 33FF6D064E59343942520343
ST-LINK FW : V2J33S7
Voltage : 3.20V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x410
Device name : STM32F101/F102/F103 Medium-density
Flash size : 63.999 MBytes
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_JSWBJu.srec
File : ST-LINK_GDB_server_JSWBJu.srec
Size : 9716 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 9]
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.0.0.201904021149/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Error! Failed to read target status
Debugger connection lost.
Shutting down...
Thanks !
2022-08-25 11:56 AM
I was having similar problems after I updated STM32CubeIDE from 1.9.0 to 1.10.1 but I had also seen it after I installed v1.9.0 too and forgot how I fixed it.
Basically, the IDE tries to run STLink at 24000 kHz which my target did not seem to like. I reduced it to 21000 kHz and things worked properly.
To set it, in the IDE with the project loaded, right click on the project name in the Project Explorer window. Properties->Run/Debug Settings. Select the project name and then 'Edit'. Under the 'Debugger' tab you can find the interface frequency.
My suspicion is that when I updated the IDE to 1.10.1 it reset the STLink frequency back to the default clock speed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.