STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Program fixed memory Area with cube Programmer

Hi,I have realized a project for Stm32G0B1 device. In my project I put a marker at address 0x807fff0. If I program the chip using keil I don't have any issue but if I use Stm32Cube Programmer the marker memory is not programmed. Is there anything to ...

Resolved! STM32G030F6P6 can't programming

I can control the card with stm32 CubeProgrammer when I reset mode "hardware reset". But when I use cubeIDE, I can't assign the program, it can't see the target, what could be the reason? Can I only use it in Hex mode?

buccno by Associate II
  • 2283 Views
  • 3 replies
  • 0 kudos

Error: failed to erase memory

Good afternoon, I was trying to debug a program on my new stm32f103C8T6 chip using the st-link v2 programmer, but i always get the same error : Error: failed to erase memoryI have tried the procedure with multiple boards so i guess that the problem i...

ABouk by Associate II
  • 26533 Views
  • 20 replies
  • 0 kudos

Resolved! How do I get a positive response from the bldr write memory command if it then the data is not properly written at the memory location? And this only happens in one out of dozen devices of the same model.!

Hello,I am facing a problem for the first time with one device while doing something that has worked perfectly on several (dozens) before of the same model (STM32H755IIT6).I am updating the firmware of the device with a custom update tool that has cl...

JPatr.3 by Associate II
  • 1816 Views
  • 2 replies
  • 0 kudos

Resolved! External Memory Loader

Hello,I want to learn how to write my own octospi external memory loader in STM32CubeIDE. I found example on https://github.com/STMicroelectronics/stm32-external-loader/tree/main/STM32H7x_boards/MX25LM51245G_STM32H735G-DK but project is built with EW...

Louise by Associate II
  • 4377 Views
  • 2 replies
  • 0 kudos

Resolved! How do I re-program the STM32G0B1RET6 after I've done a "Full chip erase" in CubeProgrammer?

Hello i have a SKR board and the MCU was faulty. I swap the chip and tried to conect via SWD on CubeProgrammer but no success after i have can connect via usb but when i as to program by my mistake i erase full chip and after cannot conect again.Is t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.