STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

DFU STM32H7S7L8 + External Loader

Hello,I'm working with the STM32H7S7L8 -DK and I need for final product to program the external OCTOSPI flash via usb DFU.So using V2.20.0 Cube programmer i'm able to use external memory loader to read and program the flash using SWDBut using the USB...

Hamady by Senior
  • 686 Views
  • 5 replies
  • 2 kudos

Resolved! DEV_USB_COMM_ERR for REAL St-link V2

I bought an ST-link V2 from amazon, this error occured, fearing it may be counterfeit, I then bought another St-link v2 from STM website itself so there is no way it is fake, but the same error still occured. I am on Mac M3 using Cubeprogrammer. Ther...

OWENL by Associate II
  • 1491 Views
  • 8 replies
  • 2 kudos

STM32N6 .tsv file with application

Hello,What is the correct layout for the .tsv file for the STM32N6 with application?In this tutorial the FlashLayout.tsv is shown, however it only has the FSBL program in it. I cannot figure out what Id to use for the Appli (also Appli non secure), i...

Tuomas95 by Associate III
  • 372 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.