STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Cannot connect to STM32H747BIT6 anymore

I have been running into an issue with the cubeprogrammer very recently where I am unable to connect to my MCU anymore. I get the following log: using v2.2212:41:28 : STM32CubeProgrammer API v2.22.0 | Windows-64Bits12:43:17 : UR connection mode is de...

peter627 by Associate II
  • 752 Views
  • 7 replies
  • 0 kudos

Resolved! [BUG][V2.20] -noreconnect doesnt work on Windows

I recently tried to use -noreconnect via the cli on windows and it still attempted to reconnect.I was connected via UART and programming option bytes. Here was the command I used:& "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bi...

dnugent by Associate II
  • 1407 Views
  • 8 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.