STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer 2.16 - cannot program MCU by USB

Hello,After installing STM32CubeProgrammer v2.16, I was unable to program a STM32F412 by USB (in DFU mode).I've never had a problem doing this and after uninstalling v2.16 and installing v2.15, everything worked fine.This problem was also confirmed b...

STeve-o by Associate
  • 2188 Views
  • 3 replies
  • 0 kudos

STM32CubeProgrammer 2.16.0 crashing in SWV

Hello,I'm using STM32CubeProgrammer version 2.16.0. The debugging works fine, but if the connection with the target is lost or probably some bad message is received on the client side, the application crashes. So in the first place I can't even see t...

krasl by Associate
  • 1050 Views
  • 0 replies
  • 0 kudos

CubeProgrammer 2.16 CLI problem - warning

After upgrading CubeProgrammer to new release 2.16 CLI commands started to fail during verification phase when changing option bytes on STM32U5A5. Sample command which fails:STM32_Programmer_CLI -c port=SWD mode=UR --hardRst -ob WRP1A_PSTRT=0xff WRP1...

TDJ by Lead
  • 1212 Views
  • 1 replies
  • 0 kudos

Unable to connect to STM32L452REY6

Hello Team,We are facing an issue while programming our MCU from STM32Cube Programmer. The error we are having is shared below:18:50:44 : ST-LINK SN : 36FF7006564834385641104318:50:44 : ST-LINK FW : V2J43S718:50:44 : Board : --18:50:44 : Voltage : 3....

Ashu123_0-1707830557056.png
Ashu123 by Associate
  • 1378 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.