2024-04-08 8:11 AM
Hello,
I'm using STM32CubeProgrammer version 2.16.0. The debugging works fine, but if the connection with the target is lost or probably some bad message is received on the client side, the application crashes. So in the first place I can't even see the last SWO messages that were received from the target.
Hardware: STM32U585 - SWD - HW Reset - ST-Link V2.0 ISOL @ V2J43S7
System log attached.
thx,
- Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.