STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! How to program STM32H563ZI with TZ disabled using CLI?

Hi,I'm trying to program a hex file generated with 'TrustZone disabled' software model targeting STM32H563ZIT6 (NUCLEO-h563ZI) as:"C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=SWD freq=4000 s...

WCarey_0-1711945173625.png WCarey_1-1711945550252.png
WCarey by Associate III
  • 1912 Views
  • 1 replies
  • 0 kudos

Resolved! External loader for STM32WL5: code is not loaded in ram

Hello,I'm trying to develop a custom external loader for STM32WL5 device, in a custom board using SPI flash memory Winbond W25Q80DV.In the past I've already developed external loaders successfully for other MCUs and boards.I again followed the steps ...

LorVec81 by Associate II
  • 6863 Views
  • 6 replies
  • 0 kudos

UR connection mode is defined with the HWrst reset mode

Hello all developers Today I came to ask for advice. I have an STM32 Nucleo-144 development board with stm32H723ZG. At first it worked fine. But suddenly there was a problem of not being able to connect to the stm32cube programmer. I was wondering wh...

non_0-1709705540926.png non_1-1709705562660.png 46991.jpg
non by Associate III
  • 10751 Views
  • 1 replies
  • 0 kudos

Troubleshooting CUBE Programmar Settings Change Error

I briefly changed the option byte setting through CUBE ProgrammmerIt was changed well before, but I tried to change the DMEP setting and return it because I couldn't want it, but an error occurred and it is not changing The error appears as follows, ...

04.JPG
ark2 by Associate III
  • 1014 Views
  • 0 replies
  • 0 kudos

Multi Board Programming

Hi,I have 20 boards in a 4x5 panel board. all boards have the same MCU. is it possible to program all boards via a panel at the same time? if so, how can I do that? which software and hardware tools do I need?Thank you.

mehmetk by Associate
  • 1669 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.