STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32Cube Programmer API USB Example error

Hello,I put my STM32H743XI in Bootloader mode and launch STM32Cube Programmer USB example on VS and got : I have two question :Where does this error comes from and how to fix it ?Can I skip option bytes programming and still flash my MCU ?Regards

0693W0000059bznQAA.png

Resolved! STM32CubeProgrammer Install/Uninstall issues. I can't uninstall the previous version of the Programmer. The newly installed version won't run.

Trying to uninstall the previous version, I get: "Windows cannot find C\Program Files (x86)\Java\jre1.8.0_251\bin\javaw.exe. Trying to run the newly installed Programmer, I get "CubeProgrammer_API or one its dependencies is missing. Please try reinst...

Resolved! Error to connect to target STM32H747I-DISCO

I try to connect to target STM32H747I-DISCO but show this message:08:58:19 : ST-LINK SN : 004800413137510D3938353808:58:19 : ST-LINK FW : V3J3M208:58:19 : Voltage : 3.27V08:58:19 : No STM32 target found!08:58:20 : ST-LINK SN : 004800413137510D393835...

Programming STM32F405 in bootloader mode via stm32cube programmer command line interface at the address 0x08008000, the programming processes completes successfully but the controller does nothing afterwards I don't understand why?

I am student developing an app that uses the STM32CubeProgrammer command line interface executable to program STM32F405.The controller works as excepted if it is programmed at the address 0x08000000.but sometimes the programming processes fails or st...

Resolved! Deadlock on STM32H745I-Disco board and it Throws error "No STM32 target Found" in STM32CubeProgrammer

Deadlock on STM32H745I-Disco board .The STM32H745I-Disco board Throws error "No STM32 target Found" in STM32CubeProgrammer . Can we recover this Board if the TAG connector is connected to SEGGER DEBUG Adapter 11:10:20 : STM32CubeProgrammer API v2.5.0...

0693W000004JZZjQAO.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.