STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Can't build API examples. Library issues! Help!

:-1: error: /home/serg/STMicroelectronics/STM32Cube/STM32CubeProgrammer/api/project/Qt/STM32CubePrgAPI/../../../../lib//./libQt5Xml.so.5: undefined reference to `QXmlUtils::isPublicID(QString const&)@Qt_5_PRIVATE_API'Qt Creator 4.7.1Based on Qt 5.11....

SSolo.2 by Associate II
  • 1499 Views
  • 0 replies
  • 0 kudos

stm32l515cb no debug with gdb only openocd

We can not user gdb for debug with our board. We can not user stm32programmer eitherIt works correctly with stlink and debug with openocd.the strange thing is that stm32cube programmer connects correctly to the device but recognizes it as stm32l0.wha...

0693W0000059tJbQAI.png 0693W0000059tJpQAI.png
PVale.2 by Associate
  • 634 Views
  • 0 replies
  • 0 kudos

I have installed the latest (en.stm32cubeprog_v2-3-0) version in Windows 10 64 bit PC. After installation, the first startup icon with spinner only comes up , closes and does not run. As far as googled and found online, it is java versioning issue.

I have installed the latest (en.stm32cubeprog_v2-3-0) version in Windows 10 64 bit PC.After installation, the first startup icon with spinner only comes up , closes and does not run.As far as googled and found online, it is java versioning issue. Thi...

PPK by Associate II
  • 1087 Views
  • 1 replies
  • 0 kudos

STM32CubeProgrammer gives me an error

I'm trying to program STM32L031 microcontroller using STLINK but STM32CubeProgrammer gives me the following error:Error: No STM32 target found!These are the conditions:1) The hardware is correctly connected because the STM32CubeIde emulates correctly...

PNenn.1 by Associate
  • 1143 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.