STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

I am not able to start STM32CubeProgrammer even installed Oracle JDK 13.0.1 and openjfx. What's the problem?

I am not able to start STM32CubeProgrammer even installed Oracle JDK 13.0.1 and openjfx:System: Ubuntu 18.04 VirtualBox on MacOS 10.15: ~$ STM32CubeProgrammerError: Could not find or load main class com.st.app.MainCaused by: java.lang.NoClassDefFound...

JasonZ by Associate II
  • 4253 Views
  • 8 replies
  • 1 kudos

Why it is fail to program using st-link-v2 with stm32cubeprogrammer MCU family STM32F09x/F030xc using SWD port

17:23:22 : Address : 0x00000224 17:23:22 : Erasing memory corresponding to segment 0:17:23:22 : Erasing memory corresponding to segment 1:17:23:22 : Erasing internal memory sector 017:23:22 : Erasing memory corresponding to segment 2:17:23:22 : Erasi...

CCai.1 by Associate
  • 1703 Views
  • 3 replies
  • 0 kudos

Resolved! Installintg CubeProgrammer (java issue)

Hello,I am running new windows 10 fresh install on my laptop, having issue installing BOTH CubeMX AND Cubeprog, either one of them does not launch or install or the other one does not install or launch.If I go with java OpenJDK 8, the Cubeprog works ...

0693W000004JBNZQA4.jpg
LBeau.1 by Associate III
  • 3170 Views
  • 5 replies
  • 0 kudos

STM32VLDISCOVERY (DEVICE_NOT_SUPPORTED)

Hello,I am using Ubuntu 18.04 LTS and CLI version of STM32CubeProgrammer 2.5.0.My board is STM32VLDISCOVERY with STM32F100RBT6 MCU. When I do list devices or connect, I get DEVICE_NOT_SUPPORTED. Attaching log.Thanks,Mitul

MMeva.1 by Associate II
  • 2760 Views
  • 4 replies
  • 0 kudos

STM32L562E-DK Failed to connect.

Hello STM team,I am working with STM32L562E-DK. It was working fine, but suddenly the STM32L562E-DK is failing to connect. And generates a FAIL.TXT which says "The interface firmware FAILED to reset/halt the target MCU".NOTE: I have not done any modi...

Neel by Associate III
  • 1463 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.