STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

External loader STM32L442 and S25FL127 Cypress

Hello all,I have written a External Loader using nucleo-l476rg and S25FL127 16mb NOR flash using 64k sectors. I was using it with TouchGFX and it worked just fine. I migrated to stm32l442. I have copied the code for the flash driver, changed the lin...

Future of STM32CubeProgrammer

Hi, I have a couple questions about the future of the programmer. 1) Are you planning to add self updating at any time? 2) This is really close to being a useful programmer on the production line. Basically it needs a way to save a configuration fo...

Resolved! Cann't open STM32_Programmer_CLI.exe

I have installed STM32CubeProgrammer 2.7.0 on Windows 10 and it works fine. but when iam trying to run STM32_Programmer_CLI.exe even as admin it open and close immediately. the same thing happens by openning the STM32Bootloader.batCould anyone tell m...

Dalhe.1 by Associate II
  • 14443 Views
  • 8 replies
  • 1 kudos

Resolved! ST-LINK_CLI.exe no full support for STM32G43x?

Hello, I was trying to set option bytes (BOR) with the ST-Link CLI (v3.6.0.0) for STM32G431, but it prompts that this feature is not available. With the ST-LINK Utility (v4.6.0.0) it is possible to set the BOR Level.I guess the ST-Link CLI is no long...

0693W00000AP9JCQA1.png
DKinz.1 by Associate
  • 1387 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer cannot connect to NUCLEO-F207ZG board in bootloader mode via UART interface

I have a NUCLEO-F207ZG board and STM32CubeProgrammer v2.7.0. I would like to use the embedded bootloader located in system memory. So, first I activate bootloader mode pulling-up pin 138 (boot0) of the MCU. Then, in order to verify this first operati...

RConf.1 by Associate II
  • 2325 Views
  • 1 replies
  • 0 kudos

Resolved! RAM parity function on the STM32G071RB breaks code execution? In short: When i clear the RAM_PARITY_CHECK bit in the option bytes (FLASH_OPTR bit 22), the program (in flash) will not run. Is this a hardware bug or am i doing something wrong?

I'm working on the NUCLEO-G071RB development board, using the IAR-EWARM (8.50.9) tool-chain.I've created a very basic program that only toggles user led (LD4) at 500ms intervals (using a wait loop with NOP instructions).The program doesn't use RAM (h...

EScho.2 by Associate
  • 2301 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.