STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STMCubeProgrammer will not start

I just installed en.stm32cubeprg-win64_v2-7-0.zip.Installation went without problems but when I try to start the application I get the splash screen and then it just exits apparently. If I runt it from a prompt I get no messages.C:\Program Files\STMi...

Setting Auto mode with STM32CubeProgrammer v2.7.0

I have just started using STM32CubeProgrammer v2.7.0 and I liked the simple and great looking UI over the other programmers. Now I would like to use Automatic mode and expect the following:Erase the Read Out Protection (RDP) in OB or set it to "AA"Fu...

JABRA.1 by Associate II
  • 5690 Views
  • 9 replies
  • 0 kudos

FDCAN programming support?

As far as I can tell, cube programmer supports programming over CAN, but not FDCAN, like on the newest MCUs. True? Is there a path for STLink and cube programmer to support FDCAN?

MMedv by Associate II
  • 1762 Views
  • 1 replies
  • 0 kudos

Programming via UART

Hello,I am trying to program Nucleo- H743ZI2 via UART (UART3) according to AN2606 doc page 244.I have managed to successfully program small bin and elf files. However, when I try to program a bigger file (bin = 655,619KB, elf = 5870KB) I am getting a...

IShar.2 by Associate II
  • 794 Views
  • 0 replies
  • 0 kudos

STM32 QSPI external flash loader issue

Hi.In a project I'm working on, I have to use external flash because the internal flash memory is low.I decided to use the MT25QU512ABB chip as it supports QSPI. After some research on the internet, I found the video of STMicroelectronics on youtube ...

johnLocke by Associate II
  • 4041 Views
  • 5 replies
  • 0 kudos

Resolved! STM32CubeProgrammer v2.7.0-RC1 doesn't find target.

I am trying to debug small project on STM32H7B. I use STM32 Cube Programmer and STLINK-V3SET to clear the flash. It seems to me that ST-LINK GDB server ver 5.8.0 is connected. See blow.==========STMicroelectronics ST-LINK GDB server. Version 5.8.0...

NNari.1 by Associate II
  • 3142 Views
  • 4 replies
  • 0 kudos

Help connecting to STM32 on Cube Programmer

Hello everyone,I have a PCB with an embedded STM32F103 on it. The PCB provides access to some ports on the side. Those are linked to VDD, PA9, PA10, PA13, PA14 and GND. I tried connecting to it with Cube Programmer using a FT232RL as pictured below :...

0693W00000BZseOQAT.jpg 0693W00000BZsfRQAT.jpg 0693W00000BZsdqQAD.png
Math86 by Associate II
  • 5830 Views
  • 8 replies
  • 0 kudos

Resolved! CubeProgrammer UART Bootloader Error

Using STM32F412RGT6 on a board I've developed.having a problem using bootloader via UART (using CubeProgrammer).Following all described in AN2606.In my application, I'm using bootloader via UART1 (PA9, PA10).BOOT0 is High, BOOT1 is low while attempt ...

JUker by Associate II
  • 1632 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.