STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32H745XI Dual Core External Bootloader

Hello,I have developed a external Loader for my custom projekt. It uses a W25Q128 QSPI conected to bank 2 and alternative Pin of CLK. (Worse!, but it is so...) So i Have no exactly example for it. Also it is a Dual Core, and no example i find have sp...

user4711 by Associate II
  • 12387 Views
  • 10 replies
  • 1 kudos

ST-LINK2 on Windows 11

I have worked with ST-LINK/2 on Windows 10 for several years. I must upgrade to Windows 11 because Windows 10 support ended a few months ago. Today, I tried to program the WIO E5 Mini microcontroller, but I found it's impossible because there's no dr...

markpow by Senior
  • 1417 Views
  • 20 replies
  • 5 kudos

Resolved! Fails to program after DFU

I have been working with a custom board using the STM32U073 for while, and have made a program that can active the USB system memory DFU. After this I suddenly cannot program the board anymore using the STM32CubeProgrammer.I can read all the flash me...

JJust.2 by Associate II
  • 764 Views
  • 3 replies
  • 1 kudos

Resolved! HSM reader detection

Hi, using STM32 Cube Programmer and STM32 Trusted Package Creator W2.21, I was unable to detect the HSM card, getting error 0x88000002. I had to downgrade to V2.14, as mentionned in several posts to get it detected successfully.I use HID Omnikey 3121...

PLencou by Associate
  • 498 Views
  • 2 replies
  • 1 kudos

Resolved! STM32CubeProgrammer cannot read UID via UART

The STM32CubeProgrammer does not appear to be able to read system memory from an STM32L051 when using the UART interface however it is able to do so when using the SWD interface.  When using the UART interface, both flash and EEPROM can be read, but ...

DAlbe.3 by Senior II
  • 371 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.