2024-05-16 7:06 AM - edited 2024-05-16 8:23 AM
Hello,
I have developed a external Loader for my custom projekt. It uses a W25Q128 QSPI conected to bank 2 and alternative Pin of CLK. (Worse!, but it is so...) So i Have no exactly example for it. Also it is a Dual Core, and no example i find have special definitions for it.
I worked more days on it and it worked perfekt (now!) in a Cube Projekt.
Erase, write and read (manual) and memory mapped mode are perfect.
If I compile the stldr file, I can load ist in Cube programmer and stm prog utility.
But then I could cry. I can't do anything. No read on QSPI and so on.
....
I think i will have trouble with the m4 Core. The M7 Core must wait for him.
I don't know. How you can help me. What is wrong. Have you any Idea?
2024-05-16 7:09 AM - edited 2024-05-16 8:30 AM
2024-05-20 11:53 AM
Have anyone an Idea?
2024-05-20 12:19 PM - edited 2024-05-20 5:17 PM
The Bus Matrix has the QUADSPI on the CM7 side, that's where the code is running.
I don't see that being on BANK2 (BK2) would introduce any particular issues.
PB2:AF9 CLK
PC11:AF9 NCS
PH2:AF9 D0
PH3:AF9 D1
PG9:AF9 D2
PG14:AF9 D3
I'd probably look at how it's build, and the .LD for the single core H7 would suffice. https://github.com/cturvey/stm32extldr/blob/main/ExternalLoader.ld
I would not use or create dependencies on Interrupts, Vector Table, startup.s initialization nor main() entry.
I'll map your pin definitions into an existing build and see where it gets us..
2024-05-20 5:09 PM
2024-05-21 12:04 AM
Super great, thank you. But can you tell me how you did it. The file is only 8kb! I would like to modify the whole thing and integrate LEDs and other tasks.
Can you send me the relevant files as source code so that I can make a cube project.
Thanks again
2024-05-21 1:02 AM
It is part of a larger project for which source is not generally provided.
The files are smaller as a lot of junk and dead code has been removed, but is basically an optimal HAL implementation in GNU/GCC
2026-01-16 5:38 AM
Can you provide dual core external loader source code for reference.
2026-01-16 5:46 AM
@user4711 have you got the source code?
2026-01-16 5:48 AM
Facing same issue
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.