STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

External Flash Loader on STM32G474 with SPI.

Hi,I'm trying to migrate an old firmware from a STM32F303 to a STM32G474.The MCU is related to an external Flash W25Q16JV.The old configuration uses the SPI bus to communicate with the external flash.So I changed the program in order to adapt the new...

MAmem.1 by Associate III
  • 1876 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to connect to STM32H7 system bootloader via UART

I have been working with STM32H753 device. I was able to boot into the system booltoader of the Nucleo board. Cube Programmer was able to detect and connect through UART.But, I am unable to connect the Cube programmer in our custom board. Both BOOT_A...

SP.12 by Associate II
  • 3700 Views
  • 4 replies
  • 0 kudos

I tried to program STM32F407 MCUs, using STLINK-V3MINI and STM32CubeProgrammer in automatic mode, but after first MCU, I'was not able to program any other MCUs. Someone could help me?

This is the log: 16:37:14 : STM32CubeProgrammer API v2.8.0 16:37:32 : ST-LINK SN : 003500125553500D20393256 16:37:32 : ST-LINK FW : V3J8M3 16:37:32 : Board    : STLINK-V3MINI 16:37:32 : Voltage   : 3.00V 16:37:32 : SWD freq  : 24000 KHz 16:37:32 : Co...

FCiuc.1 by Associate
  • 1171 Views
  • 1 replies
  • 0 kudos

Cannot Open file in STM32CubeProgrammer

Before this all work fine until suddenly the file cannot be open. Tried to uninstall and delete all related file form pc then install back. Tried also to download the new and old version. The result in the same for both, still cannot open file. Can s...

SBint.1 by Associate
  • 2271 Views
  • 4 replies
  • 0 kudos

STM32CubeProgrammer 2.10.0 released

STM32CubeProgrammer v2.10.0 release information New features • Added the updater tool for automatic software updates. The updater allows the users to make automatic updates of the software and its associated packages. It is available in all supported...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.