2022-06-03 9:11 AM
Hi,
the Serial wire viewer (SWV) has a command-line option.
This only launch the viewer and the user has to press R to start.
Is it possible to directly start the SWV?
Or is there a shell trick for this?
- Thomas
*********************************************
Manual
STM32_Programmer_CLI.exe -c port=swd -swv freq=32 portnumber=0
C:\Users\ST\swvLog\example.log
Serial wire viewer (SWV) command
-SWV
Description: This command allows the user to access the serial wire viewer console mode,
which displays the printf data sent from the target through SWO.
In this mode (see Figure 105) the user can start and stop the reception of the SWO data by pressing, respectively, the “R�? and “S�? buttons on the keyboard. T
Solved! Go to Solution.
2022-07-01 3:38 AM
Hello @Bacteriuslocher,
Thank you for posting,
You can use the option -RA along with the command you mentioned in order to start the CLI SWV automatically.
If you have any further questions, do not hesitate to ask.
Best regards,
Aziz
2022-07-01 3:38 AM
Hello @Bacteriuslocher,
Thank you for posting,
You can use the option -RA along with the command you mentioned in order to start the CLI SWV automatically.
If you have any further questions, do not hesitate to ask.
Best regards,
Aziz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.