STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Help to put stm32 32f042 in boot mode

Help to put stm32 32f042 in boot mode.I have this board from aliexpress and i want to load a project with STM32CubeProgrammerhttps://www.aliexpress.com/item/1005001417495721.html?spm=a2g0o.order_list.0.0.21ef18026yFGOLI receive this error and i think...

mm.4 by Associate II
  • 3850 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeProgrammer does not work with Windows 11.

I have the following problem. I recently installed Windows 11 and tried to install the STM32CubeProgrammer. But non of the following versions work with Windows 11STM32CubeProgrammer 2.11.0STM32CubeProgrammer 2.10.0STM32CubeProgrammer 2.9.0I always ge...

0693W00000Sv9rAQAR.png
TWolf.2 by Associate
  • 3611 Views
  • 2 replies
  • 0 kudos

MCU STM32F733ZE doesn't START

Hello Community,We have an issue on a design with an MCU STM32F733ZE on a custom electronic board, we don't manage to program it through STM32Cubre Programmer ("No STM32 found"). We observed that the power consumption is very low, less than 0.1mA so ...

SFELL.1 by Associate II
  • 4498 Views
  • 6 replies
  • 0 kudos

Resolved! STM32L4Q5CGT - not detecting in STM cube programmer

Hi All,We had purchased STM32L4Q5CGT6 controller for our work and after assembling and testing programming using STLINK V3 using SWD we found that none of the controllers are being detected in the programmer software. when connected the following scr...

PJose.3 by Associate II
  • 4267 Views
  • 9 replies
  • 0 kudos

Resolved! STM32_Programmer_CLI on Ubuntu

Hi,I use STM32_Programmer_CLI.exe on windows. I can use it from python like that:process = subprocess.Popen( ["STM32_Programmer_CLI.exe","-l"], text = True,shell=True, cwd=self.cubeProgPath,stdout=subprocess.PIPE)How c...

JJRR by Senior
  • 3396 Views
  • 1 replies
  • 0 kudos

STM32F767 dual boot option from flash memory

Hey everyone,I'm using the STM32F767 and trying to use the dual boot option to load and run a new image from the flash memory.Using the stm32CubeProgrammer, I have changed the nDBANK and nDBOOT bits to enable those options. Also downloaded the binary...

0693W00000StfJaQAJ.png
gsaru.1 by Associate II
  • 1968 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.