2022-08-16 1:34 PM
Hello i have a SKR board and the MCU was faulty. I swap the chip and tried to conect via SWD on CubeProgrammer but no success after i have can connect via usb but when i as to program by my mistake i erase full chip and after cannot conect again.
Is there some way to conect the chip or is broke?
Solved! Go to Solution.
2022-08-16 4:50 PM
Pull up BOOT0 (SWCLK) to VDD and connect in USB DFU mode.
By the way, looking at that schematics...
2022-08-16 3:08 PM
>>Is there some way to connect the chip or is broke?
No idea, not my board, got a schematic?
The ST-LINK would likely need VCC-TARGET, GND, SWDIO, SWCLK and NRST.
Try Connect Under Reset options
Try Slower SWD clock speeds for CM0(+) parts
2022-08-16 3:10 PM
If BOOT0 pin is pulled HIGH, can it connect to PC via USB as "STM32 BOOT DEVICE" type of thing? If so FW could perhaps be pushed by USB/DFU mode in STM32 Cube Programmer.
Talk to the Vendor, Read ALL the instructions.
2022-08-16 4:50 PM
Pull up BOOT0 (SWCLK) to VDD and connect in USB DFU mode.
By the way, looking at that schematics...
2022-08-18 6:35 AM
Tanks for the help
I have can write the chip again.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.