2022-08-20 2:08 AM
Hello,
I want to learn how to write my own octospi external memory loader in STM32CubeIDE. I found example on https://github.com/STMicroelectronics/stm32-external-loader/tree/main/STM32H7x_boards/MX25LM51245G_STM32H735G-DK but project is built with EWARM or MDK-ARM IDE.
I generated new project and configured octospi interface in CubeIDE. Then I added files from this repository to communicate with the memory. Then I copied linker file from this repository: https://github.com/STMicroelectronics/stm32-external-loader/tree/contrib/Loader_Files/H7%20device
I generated .stldr file according to this video: https://www.youtube.com/watch?v=XqCq0xtQmbI&t=2s&ab_channel=STMicroelectronics, but when I added this file to STM32CubeProgrammer it shows error: Data read failed.
I know that octospi interface is configured well because I can write bytes to memory and then read it by default external loader. I can also read mem ID which is C2 85 3A
Whether these problems are caused by the linker file or should I change anything else in the project?
Is there any way to convert IAR project to STM32CubeIde project?
Best Regards
Solved! Go to Solution.
2022-08-22 12:59 AM
Thanks for your reply,
I have already solved the problem. I changed #define KeepInCompilation __root to #define KeepInCompilation __attribute__((used)) instead of deleting it.
2022-08-20 8:00 AM
This is my GNU/GCC linker script, for the loaders I build via a makefile and the tools directly. I'm not using CubeIDE
https://github.com/cturvey/stm32extldr/blob/main/ExternalLoader.ld
The loaders don't start/enter via the startup.s / main() route, consequently the data/bss sections will not be moved or the zero-space initialized. Be wary of this
Porting from IAR or KEIL shouldn't be too difficult. The loader projects are pretty flat, most of mine contain the HAL include files, a handful of HAL source files, and a pair of loader source files.
Debugging of the loader can't be done directly, you'd either need to wrap it in some harness or instrument it to use interfaces on your board.
Notes to self
OCTOSPI1 GPIO Configuration
PF10 ------> OCTOSPIM_P1_CLK AF9
PG6 ------> OCTOSPIM_P1_NCS AF10
PB2 ------> OCTOSPIM_P1_DQS AF10
PD11 ------> OCTOSPIM_P1_IO0 AF9
PD12 ------> OCTOSPIM_P1_IO1 AF9
PE2 ------> OCTOSPIM_P1_IO2 AF9
PD13 ------> OCTOSPIM_P1_IO3 AF9
PD4 ------> OCTOSPIM_P1_IO4 AF10
PD5 ------> OCTOSPIM_P1_IO5 AF10
PG9 ------> OCTOSPIM_P1_IO6 AF9
PD7 ------> OCTOSPIM_P1_IO7 AF10
2022-08-22 12:59 AM
Thanks for your reply,
I have already solved the problem. I changed #define KeepInCompilation __root to #define KeepInCompilation __attribute__((used)) instead of deleting it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.