STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Did I brick my STM32F2?

Hi all -I'm modifying some legacy code written for a WICED device that contains an STM32F2xx. The original programmer had a passage that reduces down to:#define OB_RDP_Level_0 ((uint8_t)0xAA) #define OB_RDP_Level_1 ((uint8_t)0x55)   FLASH_OB_Unlo...

mzimmers by Associate II
  • 2180 Views
  • 2 replies
  • 0 kudos

Error: Download verification failed

hii am using STM32H745BIT6, i am using a st-link v2. i was able to debug until Friday but suddenly it stopped and gives me this error.STMicroelectronics ST-LINK GDB server. Version 7.0.0Copyright (c) 2022, STMicroelectronics. All rights reserved.Star...

fMoha.1 by Associate II
  • 1772 Views
  • 1 replies
  • 0 kudos

How to use the program load header for the debug environment flash algorithm while using the STM32CubeIDE?

Hi there,it seems that STM32CubeProgrammer (Version 2.6.0) is using the program load header information to flash the system, while the STM32CubeIDE (Version 1.8.0) is using the section information. Since the initialize data section is not part of tha...

BMäme.1 by Associate II
  • 3095 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.