2022-07-05 11:16 AM
hi
i am using STM32H745BIT6, i am using a st-link v2. i was able to debug until Friday but suddenly it stopped and gives me this error.
STMicroelectronics ST-LINK GDB server. Version 7.0.0
Copyright (c) 2022, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.11.0-RC1
-------------------------------------------------------------------
Log output file: C:\Users\FMOHAM~1\AppData\Local\Temp\STM32CubeProgrammer_a43060.log
ST-LINK SN : 30FF6F065647373734141043
ST-LINK FW : V2J40S7
Board : --
Voltage : 2.56V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x90
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a43060.srec
File : ST-LINK_GDB_server_a43060.srec
Size : 7.86 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:04.169
Verifying ...
Error: Data mismatch found at address 0x08000000 (byte = 0xFF instead of 0x00)
Error: Download verification failed
(Read)Failed determine breakpoint type
Shutting down...
Exit.
i check the wiring and even got a new blaster but still same.
i am using stm32ide.
2022-09-26 11:23 PM
Even I am facing the same error dont know where the problem is... ?
Is it a debugger problem or a software problem any pointers ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.