STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Using a STM32H745/755 device and Cube Programmer in DFU mode connected via USB and trying to erase flash memory via Cube Programmer..

I've noticed that if the option byte for the CM7 boot address is set to 0x1FF0 (boot into bootloader), the Cube Programmer cannot erase the flash memory. If I change that option byte to 0x0800, the flash memory erases.I can erase and program the flas...

FArms.1 by Associate II
  • 4942 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer not starting

Just installed the new version 2.11.0. Never used any version of CubeProgrammer before. I am using it on Windows 10 with Java 18.0.1.1.2022-04-22. When I start it, just the start-dialog appears and disappears after some seconds. In varioius posts I h...

KBrei.1 by Associate
  • 3242 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer STM32G474 option bytes / IWDG

Dear allIf we clear the IWDG option (enable watchdog by hardware at bootup), we cannot undo this.In that case we have to use the old STM32 ST-LINK Utility tool.STM32CubeProgrammer version: v2.11.0µC: STM32G474RBT3The problem seems to be PC dependent!...

FWege.1 by Associate III
  • 3278 Views
  • 3 replies
  • 0 kudos

Resolved! setVerbosityLevel of the API

I am calling setVerbosityLevel of the API with CUBEPROGRAMMER_VER_LEVEL_NONE (0) in the C++ USB Example project supplied but the DLL routines (like connectDfuBootloader) are still outputting messages. Still there any way to stop these messages?

STM32CubeProgrammer Issue erasing sectors past 127

Using STM32CubeProgrammer V2.11.0 on Windows 10I have issues erasing sectors past 127 on the STM32L496RET6 MCU.Erasing sectors 0-127 appears to work okay.Erasing sectors 128-255 does not show an error, however when I re-connect the programmer to the ...

Sde B.1 by Associate
  • 1226 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.