2019-12-06 6:49 AM
I have installed STM32CubeProgrammer V2.2.1 (https://www.st.com/en/development-tools/stm32cubeprog.html) on my MacBook without problems.
When I try to run the application, the programmer icon appears in the dock for about half a second and disappears immediately.
So I tried to open the application via terminal:
Last login: Fri Dec 6 15:40:05 on ttys000
➜ ~ /Library/Internet\ Plug-Ins/JavaAppletPlugin.plugin/Contents/Home/bin/java -version
java version "1.8.0_221"
Java(TM) SE Runtime Environment (build 1.8.0_221-b11)
Java HotSpot(TM) 64-Bit Server VM (build 25.221-b11, mixed mode)
➜ ~ java -version
java version "13.0.1" 2019-10-15
Java(TM) SE Runtime Environment (build 13.0.1+9)
Java HotSpot(TM) 64-Bit Server VM (build 13.0.1+9, mixed mode, sharing)
➜ ~ sudo open /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app
Password:
LSOpenURLsWithRole() failed with error -10810 for the file /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app.And I can see error code -10810...
What can I do now?
Best regards!
Solved! Go to Solution.
2019-12-07 4:36 AM
Okay, its quite easy to get it to work (tested with macOS Catalina 10.15.1 (19B88))
Please see my post at SO!
1. To be sure you use the right java version deinstall all java versions first
~ java -version
No Java runtime present, requesting install.2. Now install " jdk-8u231-macosx-x64 "
3. After that the terminal should look like this
~ java -version
java version "1.8.0_231"
Java(TM) SE Runtime Environment (build 1.8.0_231-b11)
Java HotSpot(TM) 64-Bit Server VM (build 25.231-b11, mixed mode)4. Go to the directory where the STM32CubeProgrammer installer is located. For example
~ cd /Users/myName/Desktop/en5. Install the STM32CubeProgrammer
en sudo java -jar SetupSTM32CubeProgrammer-2.2.1.exe6. The result should be
Command line arguments:
====================
Installation started
Framework: 1.6.0_65-b14-468 (Apple Inc.)
Platform: mac_osx,version=10.15.1,arch=x86,symbolicName=null,javaVersion=1.8.0_231
Installation finished7. Now you can open the programmer app
Hope this helps!
Best Regards!
2019-12-07 4:36 AM
Okay, its quite easy to get it to work (tested with macOS Catalina 10.15.1 (19B88))
Please see my post at SO!
1. To be sure you use the right java version deinstall all java versions first
~ java -version
No Java runtime present, requesting install.2. Now install " jdk-8u231-macosx-x64 "
3. After that the terminal should look like this
~ java -version
java version "1.8.0_231"
Java(TM) SE Runtime Environment (build 1.8.0_231-b11)
Java HotSpot(TM) 64-Bit Server VM (build 25.231-b11, mixed mode)4. Go to the directory where the STM32CubeProgrammer installer is located. For example
~ cd /Users/myName/Desktop/en5. Install the STM32CubeProgrammer
en sudo java -jar SetupSTM32CubeProgrammer-2.2.1.exe6. The result should be
Command line arguments:
====================
Installation started
Framework: 1.6.0_65-b14-468 (Apple Inc.)
Platform: mac_osx,version=10.15.1,arch=x86,symbolicName=null,javaVersion=1.8.0_231
Installation finished7. Now you can open the programmer app
Hope this helps!
Best Regards!
2020-03-16 1:44 AM
unfortunately i have this problem from V1 with CubeProgrammer and IDE , not with CubeMX
the ONLY way to get it started is to execute binary file using Terminal and
“cd TO CUBEPROGRAMMER BIN DIR�?
“java -jar CUBEPROGRAMMER�?
2020-04-23 3:15 AM
Update: Tested on Mac Mini OS X El Capitan v10.11.6
DO NOT run the installer app named SetupSTM32CubeProgrammer-2.4.0.app
remove previously installer version of STM32CubeProgrammer from le App directory
preliminary: install of javaVersion=1.8.0_251
reboot
then, instead of running installer .app, the install of STM32cubeProgrammer should be proceeded by running under java : SetupSTM32CubeProgrammer-2.4.0.exe in the console (note : invoke the .exe not the .app file) by:
$ sudo java -jar SetupSTM32CubeProgrammer-2.4.0.exe
result:
a GUI window of the installer opens :
-> proceed to install
at the end of install the following message appears in the terminal console
Command line arguments:
====================
Installation started
Framework: 1.6.0_65-b14-466-11M4802 (Apple Inc.)
Platform: mac_osx,version=10.11.6,arch=x86,symbolicName=null,javaVersion=1.8.0_251
Installation finished
now STM32CubeProgrammer launches correctly from Launchpad.
Best Regards
Fred
2020-05-06 5:04 AM
Hi everyone,
Could I ask your opinion of an identical error I'm having in Catalina 10.15.4?
I have installed the newest JDK 1.8.0_251 but I already had JDK 11.0.6 which I need for another app.
So to be sure I installed it the following way:
~$ ▶ where java8
java8: aliased to /Library/Java/JavaVirtualMachines/jdk1.8.0_251.jdk/Contents/Home/bin/java
~$ ▶ sudo /Library/Java/JavaVirtualMachines/jdk1.8.0_251.jdk/Contents/Home/bin/java -DjavaVersion=1.8.0 -jar ~/Downloads/en-4/SetupSTM32CubeProgrammer-2.4.0.exe
Command line arguments:
====================
Installation started
Framework: 1.6.0_65-b14-468 (Apple Inc.)
Platform: mac_osx,version=10.15.4,arch=x86,symbolicName=null,javaVersion=1.8.0_251
Installation finishedBut when I try to run the app it closes within seconds (it is not blocked by system at least it doesn't mention it under Security settings) and I also tried running it this way:
~$ ▶ java8 -DjavaVersion=1.8.0 -jar /Applications/STMicroelectronics/STM32CubeProgrammer.app/Contents/MacOs/bin/STM32CubeProgrammerBut this ends up with an error "CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program or check your java architecture."
So what am I doing wrong? Is there a conflict between JDK 11 and JDK 8 that causes STM32CubeProgrammer to crash?
I know godlyblade wrote to uninstall all versions of Java, but I do need Java 11. Is there any way around it?
Plus, Java 11 is also installed here:
~$ ▶ ll /usr/bin/java
lrwxr-xr-x 1 root wheel 74B 7 Oct 2019 /usr/bin/java@ -> /System/Library/Frameworks/JavaVM.framework/Versions/Current/Commands/javaAnd Oracle says specifically NOT to remove it as it's part of macOS system software: https://www.java.com/en/download/help/mac_uninstall_java.xml
Thank you in advance.
Chris
2020-05-06 5:42 AM
Actually, please scratch my last comment.
I couldn't remember which app I use needed Java 11, so I decided the get rid of all the JDKs.
Then I noticed my question about /usr/bin/java is stupid, since Apple just left a hook with a message showing how to install Java for yourself.
So, now I installed JDK 1.8.0_251 from scratch and STM32CubeProgrammer runs normally. Yaaay! Thanks so much guys!
But if any of you knew how to manage to have JDK 11 and JDK 8 side by side and not trip Cube Programmer then that would help a lot. In the meantime I hope the app that needed JDK 11 was just something I installed and didn't use much...
Again, many thanks!
2021-03-01 3:28 PM
@Pascal Schröer 's answer was good but incomplete. The install process also seems to use a shell script which tries to copy the jre from an odd location
#!/bin/bash
DIR="$( cd "$( dirname "${BASH_SOURCE[0]}" )" && pwd )"
DIR_APP="$( cd "$( dirname "$DIR/../../.." )" && pwd )"
cp -R "$(PWD)/../../../jre" "$DIR/../STM32CubeProgrammer.app/"That step on line 4 fails and the program won't run. However, the jre folder is in the download folder and simply copying that jre folder into the STM32CubeProgrammer.app folder solves the problem. I sure wish that Mac support was more on the ball, although I'm grateful that I can get most things working without having to fire up Windows.
2021-03-17 9:52 AM
This does the trick even for the MacOS Big Sur. Thanks @AVoel.1 !
2021-05-14 4:53 AM
@AVoel.1 @kuberaspeaking Hello Mate, I'm having this issues as you described, When the installation is about to finish It gives me that error: "Could not find jre folder". Although when I downloaded the en folder from the STM website, it came with jre folder, STM32CubeProgrammer.exe and STM32CubeProgrammer.app, what should I do?
I have continued the installation with the erro, then inserted jre folder into STM32CuberProgrammer folder, but when running the app opens and closes
2021-06-06 11:14 AM
I have exactly the same issue, and solved by going to /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/
And right click STM32CubeProgrammer.app click on Show packages content, and paste the are folder
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.