2022-09-26 7:27 AM
Using STM32CubeProgrammer V2.11.0 on Windows 10
I have issues erasing sectors past 127 on the STM32L496RET6 MCU.
Erasing sectors 0-127 appears to work okay.
Erasing sectors 128-255 does not show an error, however when I re-connect the programmer to the MCU the data is still shown in flash.
My option bytes are set as:
WRP1A_STRT = 0x10
WRP1A_END = 0x17
WRP1B_STRT = 0xff
WRP1B_END = 0x0
2022-10-03 6:00 AM
Hi @Sde B.1 ,
the STM32L496RET only has 128 sectors per bank. I think you are attempting to erase sectors in bank 2, but these are not number 128-255, these are 0-127 in bank 2.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.