STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

UART Bootloader on STM32F04xxx

Hello!I'm trying to use the embedded bootloader on STM32F042K6T6, by UART protocol, but no luck yet. I'm using USART1 pins (PA9/PA10) and BOOT0 to a button and 3v3, so I press this button and power on my board. On STM32CubeProgrammer, I've selected m...

0693W00000VOkUTQA1.png
Peaga by Senior
  • 1894 Views
  • 2 replies
  • 0 kudos

Need help with obscure Hard Fault on reset!!

We've got a bizarre Hard Fault on STM32L452. It happens immediately after reset, and ONLY after programming our bootloader with the CubeProgrammer after doing a full chip erase. If one subsequently programs the bootloader again using the same hex fil...

0693W00000KZc2PQAT.png
AVoel.1 by Associate III
  • 6328 Views
  • 9 replies
  • 0 kudos

STM ROM Bootloader issue with STM32H745

Hello, I am facing a weird issue with accessing STM ROM bootloader for flashing.Hardware Used: STM32H745-DISCOIDE: KeilI have created a simple bootloader which jumps to ROM Bootloader at startup.startup_stm32h745xx.s: ; Reset handler Reset_Handler ...

0693W00000Uo4iWQAR.png 0693W00000Uo4j5QAB.png
HKapo.1 by Associate III
  • 1842 Views
  • 3 replies
  • 0 kudos

Failure: CubeProgrammer_API or one of its depndencies missing. Please try reinstalling the program or check your java architecture.

Hello everyone,I have the following failure. I installed the STM32 Cube Programmer on Windows 10After installation I tried to start the programm but the programm will not start and i get the failure."CubeProgrammer_API or one of its depndencies missi...

MScha.10 by Associate
  • 2878 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.