STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer 2.6.0 released

New features• Added the support for dual-core microcontrollers in the STM32WL Series• Extended the support for the STM32G0 Series to the new STM32G0Bxxx and STM32G0Cxxx microcontrollers• Added SFI support via JTAG/UART/SPI for STM32WL5xxx microcontro...

M1 MacBook Air struggles with STM32CubeProgrammer.

My MacBook Air (M1, 2020) macOS Big Sur version 11.5.1 (20G80) struggles with STM32CubeProgrammer. I deinstalled all my java updates and installed the recommended java version according to this post https://community.st.com/s/question/0D50X0000BmnqrB...

0693W00000D15LXQAZ.png 0693W00000D15MQQAZ.png
OKhal.1 by Associate
  • 3871 Views
  • 3 replies
  • 1 kudos

Resolved! Downloading a ".hex" file in dropbox or onedrive path to mcu forces stm32programmer to quit

OS : windows 10 home 64bit​stm32programmer version : 2.9There is a ".hex" file in the dropbox or onedrive path.Downloading to mcu flash forces stm32programmer to quit. If the ".hex" file is not in the dropbox or onedrive path, it is downloaded normal...

ckim.2390 by Associate II
  • 1935 Views
  • 2 replies
  • 0 kudos

Resolved! How to write EEPROM with STM32CubeProgrammer via USB?

Hi Everyone,I have a STM32L1 connected via USB in DFU-Mode.I'd like to write EEPROM, but trying to do so results in "Memory Limits Error".Using old DfuSe 3.0.6., this is possible... What am I missing? Is CubeProgrammer at all capable of writing EEPRO...

0693W00000Y9TZ0QAN.png
THein.3 by Associate II
  • 2451 Views
  • 3 replies
  • 2 kudos

I wish to store data in the flash memory of my STM32G030C8T6 microcontroller. The issue I am facing is that my data is not being stored in contiguous memory banks, but rather the banks are being skipped, as seen from the image.

I have written a small driver code for the same to store different types of data types to a memory location.The link to my code is: Yadnik1/Eeprom-Emulation-driver-STM32 (github.com) and I have taken reference from here: STM32/FLASH_PROGRAM/F1 SERIES...

0693W00000Y8sbDQAR.png
YBend.1 by Associate III
  • 7589 Views
  • 12 replies
  • 1 kudos

Resolved! STM32F429 IWDG freeze in stop mode

Hi,I'm wondering if it's possible to freeze the IWDG in stop mode for STM32F429. I couldn't find this option in the STM32CubeProgrammer. Not sure if this is feasible.Thanks,

YKuo.1 by Associate II
  • 1609 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.