STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

NVIC_SystemReset() hangs after disabling BFB2.

Hi,I'm using STM32F429 on a product. I'm doing a device firmware upgrade using the BFB2 feature. The exact steps I'm doing are:Boot from Bank1 or Bank2Erase the inactive BankWrite new FW to the inactive BankToggle BFB2Soft reset (NVIC_SystemReset())I...

0693W00000aHNR8QAO.png
YKuo.1 by Associate II
  • 1085 Views
  • 0 replies
  • 0 kudos

Resolved! External Loader Parsing Error (V2.12.0)

Hi, I have updated STM32CubeProgrammer to version 2.12.0 and our custom External Loader is not load properly anymore. In the EL section I can read "Error: Flash loader error parsing fail" and in the log I can read "Error: Flash loader 'C:\*****/MyExt...

STMCube IDE: View generated run command in console

Hello,I am troubleshooting an issue with a provisioning and testing script using the STM32_Programmer_CLI. I get "Failed to erase memory errors" in the CLI but running (as far as I can tell) the same options in CubeIDE does not generate the same erro...

CubeProgrammer couldn't find stm32l476

we are developping sensor reading board which has stm32l412 AND stm32l476RG on it. we could write program to stm32l412 through CubeProgrammer without any problem but we couldn't write to stm32l476. Please addvise possible cause. Both STM32l412/476 ha...

Resolved! CubeProgrammer 2.12 - Operation exceeds memory limits

Hello Everyone,Here is my 512kB STM32L15xxE:     -------------------------------------------------------------------                      STM32CubeProgrammer v2.12.0     -------------------------------------------------------------------USB speed  : ...

0693W00000Y9FcEQAV.png
THein.3 by Associate II
  • 6770 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.