2020-02-18 1:30 PM
the file stm32l4xx_hal_conf.h in firmware repository STM32Cube_FW_L4_V1.15.0
contains a datatype mismatch in parameter 1 between the invokation and declaration of assert_failed() :
#define assert_param(expr) ((expr) ? (void)0U : assert_failed((uint8_t *)__FILE__, __LINE__))
void assert_failed(char *file, uint32_t line);The compiler correctly warns of this mismatch when compiling stm32l4xx_hal_dma.c, stm32l4xx_hal_flash.c, stm32l4xx_hal_exti.c, stm32l4xx_hal_flash_ex.c, etc.
stm32l4xx_hal_conf.h:437:65: warning: pointer targets in passing argument 1 of 'assert_failed' differ in signedness [-Wpointer-sign]Earlier versions of stm32l4xx_hal_conf.h did not contain this mismatch:
#define assert_param(expr) ((expr) ? (void)0U : assert_failed((uint8_t *)__FILE__, __LINE__))
void assert_failed(uint8_t* file, uint32_t line);Why was this change introduced, and will it be corrected?
2020-02-26 5:59 AM
Hi @Dean Neumann ,
Could you please precise which compiler are you using?
Thanks,
Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-02-29 6:12 PM
2020-05-26 8:59 AM
Hello @Dean Neumann ,
I checked that there is no more such issue With STM32CubeMX 5.6. Please check again on your side.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-05-26 9:26 AM
Please ignore about my previous comment, I checked for STM32F0 where there is no such issue. For STM32L4, problem is still there.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-05-27 2:28 AM
Hello @Dean Neumann
Thanks for the feedback,
Issue confirmed, it will be fixed as soon as possible.
Best regards,
Nesrine
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.