STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX fails under Fedora32

After a fresh install of Fedora32 STM32CubeMX fails to start. The error msg is the same for a freshly installed 5.6.1 as for the previously installed 5.6.0 (which worked under Fedora31).Has anybody a clue how to proceed? The error message is a follow...

THoff.1 by Associate
  • 1252 Views
  • 1 replies
  • 0 kudos

STM32CubeMX version in the STM32CubeIDE

I tried this wayFile >> New >> STM32 Project From STM32CubeMX .ioc File.Selected the CubeMX .ioc fileClick FinishThen, CubeIDE says belowThis file has been generated with STM32CubeMX version '5.6.1'.Your current STM32CubeMX version is '5.6.0'.Please ...

The STM32CubeMX code generation is not properly working in case the ADC is triggered by the HRTIM timers and DMA is used to transfer the ADC values to memory.

When the file stm32f3xx_hal_msp.c is created there is a missing line in function void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc) which enables the DMA clock - ( __HAL_RCC_DMA1_CLK_ENABLE(); The STM32CubeMX generates code that enables that clock in mai...

HMay.1 by Associate
  • 1793 Views
  • 3 replies
  • 0 kudos

Resolved! Using STM32CubeMX generate code for STM32CubeIDE and than change main.c to main.cpp, and build project will show up undefined reference to 'main' error.

The error message like as:Core/Startup/startup_stm32f765vitx.o: In function `LoopFillZerobss':J:/STM32PRJ/CB_ENV/MS220_F765VI/VIDEOBOARD_V9A/20200520/Debug/../Core/Startup/startup_stm32f765vitx.s:97: undefined reference to `main'​collect2.exe: error:...

jcRuan by Associate II
  • 8549 Views
  • 6 replies
  • 0 kudos

hi guys, I'm trying to define a register range for uint32_t array. I couldn't find a place online that explain in properly. do you know a way to do so?

uint32_t REG_INIT[32];//// i dont think it is necessery that only for explanation #define MainAddr     ((uint64_t)0x801FEC0)#define step 0x8#define BiasRefInit *(uint64_t *)(MainAddr+0*step)#define BiasRefFinal *(uint64_t *)(MainAddr+1*step)#def...

Gbasi.1 by Associate II
  • 4317 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.