2020-06-29 3:16 AM
I can not use CANBUS and USB together. I configurated USB and CAN together but PC does not recognise the STM32F103C8 as an USB driver.
When I use only USB without CAN configuration then USB work properly and recognise it as an USB driver.
When I add CAN configuration from different pins (PB8 and PB9) then CANBUS works on these pins but USB not.
How can I recognise the STM32F103C8 as an USB drive to my PC with using CANBUS together? Could you help me about this please?
2020-06-29 4:57 AM
Hi @UUrcan ,
Unfortunately, you cannot use USB & CAN at the same time for the selected device. To know more about this and the why reason, please refer to this article: https://community.st.com/s/article/FAQ-Concurrent-use-of-USB-and-CAN-with-STM32F103.
Don't forget to answer the question "Was this article helpful?" from article page.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-06-29 5:10 AM
OK Amel. Thanks for your reply.
But which devices can use both of them (USB and CAN) together at the same time?
2020-06-30 9:54 AM
hi @UUrcan ,
This is applicable for low, medium-, high- and XL-density STM32F1 devices as precised in the article.
So you can select any other STM32F1 device or a device belonging to other families.
As explained in RM0008:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.