STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! How to setup SMPS Supply source in STM32CubeMX?

Hi,I want to configure my STM32H7 MCU to use SMPS configuration.I try to select RCC -> Supply Source -> PWR_DIRECT_SMPS_SUPPLY, but then get build error Src/main.c:136:26: error: 'PWR_DIRECT_SMPS_SUPPLY' undeclared (first use in this function)This is...

Tuoman by Senior II
  • 9272 Views
  • 1 replies
  • 1 kudos

Accidentally deleted program, can't restore it - very urgent

I created a CubeMX project in an important folder. I found out, that all the project files were not put inside an own folder and were all over the place. So I wanted to delete the Project to make a new one. When deleting i clicked on "delete project ...

LMess.1 by Associate
  • 2845 Views
  • 3 replies
  • 0 kudos

MBEDTLS / STM32CubeMX Broken?

I am trying to implement an MBEDTLS client based on an ST example. The MBEDTLS code fails when it tries to allocate memory using calloc. Apparently, users have been experiencing this for over a year.https://community.st.com/s/question/0D50X0000ArVXN...

CubeMX IDE v1.3.1, MacOS 10.14.6, Build fails with "/bin/sh: arm-none-eabi-objcopy.exe: command not found" - the ".exe" is incorrect.

The makefile is not correct with: arm-none-eabi-objcopy.exe -O ihex "IOproc.elf" "IOproc.hex", but the IDE is trying to run arm-none-eabi-objcopy.exe. I just reinstalled the IDE using the Mac installer - no change. How can I get the IDE to generate a...

TTeag.1 by Associate
  • 2230 Views
  • 3 replies
  • 0 kudos

Resolved! STM32Cube NUCLEO-F413ZH UART missing

Hello,I am trying to create a project with STM32Cube 5.1.0 for NUCLEO-F413ZH. I see only USART 1, 2, 3 and 6 available, none of the UARTs 4, 5, 7, 8, 9 and 10. These UARTs are available if I open a project for STM32F413ZHT, the device used in NUCLEO-...

AGoro.1 by Associate
  • 1447 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.