2021-03-20 4:29 AM
Hello Everyone, I am trying to run SDIO 1 bit mode with FATFS on a custom board but facing some issues.
1) CUBEMX Version -> 6.1.2
2) API_VERSION -> STM32Cube_FW_L4_V1.16.0
3) IDE STM32CubeIDE
4) Schematic of SD card connection is attached
I need to run SDIO 1 bit mode as I don’t have IOs left
These are the tutorials and videos I followed but I am not able to get them to work.
The following attached document contains the steps I followed. But it seems I am not able to get it working :\
No matter what I do, I always get this response -> f_open() always return (FR_NOT_READY)
Can someone please help me out here and provide some guidance? :(
2024-09-30 4:03 AM
Hello,
in the SD card diagram, pins 3 and 7 are reversed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.