STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! Incompatibility between X-CUBE-TOUCHGFX and X-CUBE-SMBUS

Hello!I'm using an STM32u5a9 with a user interface and SMBus enabled battery and charger board.CubeMX does not allow me to include both the X-CUBE-TOUCHGFX and X-CUBE-SMBUS libraries. I'm guessing there is some conflict with the I2C or how the HAL ha...

CubeMX Clock Configurator NOT Locking The Selected Values

Hi,in CubeMX clock configuration, after inputting a desired value into one of the PLL outputs (like in the LTDC Clock box) you can lock it and it turns gray (see screenshot), you can then set another related PLL output (like the DSI) and it should re...

Ricko_0-1742744286828.png
Ricko by Senior III
  • 1273 Views
  • 2 replies
  • 0 kudos

STM32G474,HRTIM,ADC

I am using hrtim to trigger the adc, but if the regular channel is not triggered with hrtim, it doesn't go into the interrupt of the ADC properly, I checked a lot of information and didn't find a solution, here is my code and cubemx configuration:   ...

iskan_0-1695029126119.png iskan_2-1695029415264.png iskan_3-1695029424941.png
iskan by Associate III
  • 1913 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.