STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX 6.14 generate OpenAMP error in STM32H747 error.

Hi all,I am using CubeMX 6.14 to generate an OpenAMP project for the STM32H747I-DISCO board. When I build the project, I receive the following warnings, and it results in an 'OpenAMP create endpoint' error at runtime. I used the same code and project...

Tom17 by Associate II
  • 3113 Views
  • 8 replies
  • 1 kudos

Update STM32CubeMX and STM32Cube MCU Packages

Hello, I want to update STM32CubeMX and STM32Cube MCU Packages, but I can't do because of the error.I tried to run STM32CubeMX in admin mode, but the error occured again.1. How do you solve this error?2. Is 'STM32Cube Updater' a real file? # Error Te...

StrangeTau_0-1744693629582.png StrangeTau_1-1744693678480.png

Resolved! STM32H7232ZG CORDIC DMA code generation issue

I would like to file a bug report for STM32CubeMX.During configuration of CORDIC using DMA, I have found the following issue:In:void HAL_CORDIC_MspInit(CORDIC_HandleTypeDef* hcordic) { if(hcordic->Instance==CORDIC) { /* USER CODE BEGIN CORDIC...

Resolved! STM32CubeMX 6.14.1 Warning without comment

Hello STM32 developers,I'm using STM32CubeMX 6.14.1 and an STM32U5G7VJTx.When clicking :Generate Code" a Warning popup appears without comment.What can be the problem?I attached the ioc file.Thanks for helping out.

Warning_unknown.png
Jack3 by Senior III
  • 1221 Views
  • 2 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.