STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Alternate pin for I2C1_SCL on STM32C011J6Mx SO8N

Hi ALLI'm playing with a STM32C011J6Mx on  a plane breakout board.Sorry if this a basic question, new to using the SMT32 , last time I played with MCUs was 6809 CPU :)I wanted to use I2C and SWD, to use both I need to move the I2C1_SCL to it's altern...

stevecimo_0-1745539731667.png stevecimo_1-1745539814793.png stevecimo_2-1745540364223.png
stevecimo by Associate III
  • 983 Views
  • 1 replies
  • 0 kudos

Going from cubeide to makefile in toolchain

I'm trying to get the BLE_p2pServer example working using a Makefile setup on an STM32WBA55CG board. I copied the .ioc file and opened it in CubeMX, changed the toolchain setting, but now I'm stuck at the "copying libraries files" stage. Not sure if ...

joarwar by Associate
  • 904 Views
  • 0 replies
  • 0 kudos

Resolved! Nucleo-N657X0-Q and CubeMX

Hi,I am using the Nucleo-N657X0-Q board and here is what I have done so far:Generated a CubeMX projectEnabled FSBL, Secure Application, Non-secure Application and ExtMemLoader projectsEnabled XSPIM, XSPI2, EXTMEM_LOADER, EXTMEM_MANAGERGenerated codeO...

fa31 by Associate III
  • 1724 Views
  • 2 replies
  • 1 kudos

STM32CubeIDE doesn't generate UART init function call

I am using NUCLEO-H743ZI which has STM32H743ZI on it. In the 'Device Configuration Tool' under the 'Project Manager'->'Advance Settings' there are options to set how I want to generate HAL calls. I basically want to set all of them 'Visibility(Static...

0693W000001qixjQAA.png
AErde.1 by Associate
  • 4344 Views
  • 6 replies
  • 0 kudos

Resolved! PLL1 HSI/HSE Bug with USB

Hi,I think I have found a bug in CubeMX v6.12.0.I have an STM32U595 with USB OTG HS.My USB peripheral is set to use the HSE as it's clock (not PLL1):However, when I try to set the oscillator source for PLL1 to the HSI, CubeMX gives an error declaring...

BCowp1_0-1745404381602.png BCowp1_1-1745404494645.png
BCowp.1 by Associate II
  • 1042 Views
  • 1 replies
  • 0 kudos

SysTick_Handler not called, STM32G0B1

I am using CubeIde for the first time.First test - run minimal program with HAL from CubeIDe Configurator, under debuggerSimple program, only SYSTICK and uart , but SysTick_Handler() is not trigged at all .And function HAL_Delay hangs because uwTick...

Xme by Associate II
  • 21258 Views
  • 23 replies
  • 7 kudos

Resolved! Udapte STM32CubeMX

Hello, I have Version STM32CubeIDE : 1.18.0, and I get a program that was communicated to me, but I have this message below :  And I downloaded and installed STM32CubeMX 6.14.1 version, but it seems that it is not taken into account in the environme...

DYann1_0-1745311554144.png DYann1_1-1745311766549.png
DYann.1 by Senior II
  • 2035 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.