STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

CubeMX Custom Queue Sizes in FreeRTOS

I am having trouble creating custom queue sizes and making them work with the Heap Usage tool within CubeMX.  But I found a workaround until the bug gets fixed.I created a queue using a custom item size (the message_data_t type is defined in my code)...

eweststrate_0-1738710049448.png eweststrate_1-1738710182293.png eweststrate_2-1738710291653.png

Resolved! STM32 CUBEMX not starting

Hi developers.I have the same issue as many others, which has been posted already 4-5 times and marked as "solved" in some of them, but it is not at all the case.The CubeMX on launsching shows the first screen (splash) and then disappears.It worked a...

kova by Associate II
  • 5265 Views
  • 8 replies
  • 7 kudos

2 bugs with VREFBUF and STM32Cube on at least STM32G491

Hi ST,There are 2 bugs in Initialization of VREFBUF.in STM32CubeIDE V1.11.0.I use FreeRTOS, but it shouldn't have any inffluence on these bugs.1.) At function main, the firsr call is to Hal Init and when VREFBuF ist activated, in function HAL_MspInit...

Osto by Senior
  • 4253 Views
  • 5 replies
  • 1 kudos

Resolved! How to make STM32F103C8T6 (blue pill) USB CDC work properly

I have such dev board and try to run it as virtual com port. I created project cubemx, enable only usb as device in CDC mode. After generating and running project with next small fixes I run it on board.int main(void){//....skip while (1) {   /* USER...

RLu by Associate
  • 3442 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.