STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Partially disabled conflict is hindering CICD pipeline

We are having a similar issue as this person here:https://community.st.com/t5/stm32cubemx-mcus/why-does-the-ioc-file-show-warnings-on-disabled-peripherals/m-p/144500/highlight/true#M5600One of the responses was that this is just a warning message and...

apseftis by Associate II
  • 1215 Views
  • 4 replies
  • 1 kudos

STM32CubeMX freezes during code generation.

Hello,I am experiencing the following issue and would appreciate your help in resolving it:When I create a new STM32 project for STM32G474CEU6 in STM32CubeIDE, main.c and other source files are not generated.The .ioc file loads correctly and the GUI ...

macalon by Associate II
  • 1096 Views
  • 1 replies
  • 0 kudos

(STM32CubeMX & Neural-ART ) atonbuf AXISRAM5 raw files

Hello,I'm trying to run a ML model (miniresnet from modelzoo) to a NUCLEO-N627X0-Q starting from STM32CubeMX (initialization of device, model & code generation). Everything is OK when i select STM32Cube.AI MCU runtime, the model is created and runs s...

Unfgr by Associate III
  • 2854 Views
  • 9 replies
  • 3 kudos

Resolved! STM32 Finder missing selectors ?

I would like to filter available products by the following specific peripherals, but those types of filters do not seem to be available.PSSIDMAMUXMDMALPDMAGPDMAHPDMASDRAM support andMinimum #of pins sized package to actually support 1 or 2+ SDRAM chi...

Using Temperature Sensor and VREFINT in STSPIN32G4 MCSDK

Hi , allI am currently working on a project using the STSPIN32G4 together with the STM32 Motor Control SDK (MCSDK). I would like to add the internal Temperature Sensor to monitor the MCU temperature.In STM32CubeMX, I have already enabled both the Tem...

1751018398428.jpg 1751018547608.jpg
1123 by Associate II
  • 1204 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.