cancel
Showing results for 
Search instead for 
Did you mean: 

Partially disabled conflict is hindering CICD pipeline

apseftis
Associate II

We are having a similar issue as this person here:

https://community.st.com/t5/stm32cubemx-mcus/why-does-the-ioc-file-show-warnings-on-disabled-peripherals/m-p/144500/highlight/true#M5600

One of the responses was that this is just a warning message and is okay.  

But I think this is causing us to have an issue with using a CICD pipeline to handle project generation. 


When I use a build script with project generate I would expect the whole process to be done without interacting with the GUI but an empty warning message actually comes up for me to click 'yes' to before it will go any further. 

 

I tried an .ioc file that I found online to test to see if it would also generate this error and it does not.  

 

I am hoping there is a way to bypass any warnings generated when doing the build using a script. Any help is very appreciated.

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @apseftis 

Could you please try to place the line below at the start of the script file:

popupwrapper set

This will prevent the popup from showing.

KR,

Souhaib

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Souhaib MAZHOUD
ST Employee

Hello @apseftis 

Could you please try the description of running STM32CubeMX in command-line mode as stated in UM1718:

"To run STM32CubeMX in command-line mode without UI, use the following command lines:

– On Windows: cd jre\bin\java -jar STM32CubeMX.exe –q 

– On Linux and macOS: ./STM32CubeMX –q"

KR,

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

That’s actually what I’m running with the build script and the dialog still pops up. It will hang until I select yes. 

Update: Well I am actually running: 

java -jar /opt/st/STM32Cube/STM32CubeMX/STM32CubeMX -q build.scr

Because if I run: 

/opt/st/STM32Cube/STM32CubeMX/STM32CubeMX -q build.scr

Then I get stuck at: 

2025-07-01 07:08:08,699 [INFO] ThirdParty:978 - Integrity check success = true
2025-07-01 07:08:08,699 [INFO] IntegrityCheckThread:100 - exiting critical section [integrity check]
2025-07-01 07:08:08,699 [INFO] IntegrityCheckThread:103 - End integrity checks thread

Which may be that warning dialog somehow still getting hung up. 

My build script is: 

config load file.ioc
SetCopyLibrary copy all
SetStructure Advanced
project generate
exit

Hello @apseftis 

Could you please try to place the line below at the start of the script file:

popupwrapper set

This will prevent the popup from showing.

KR,

Souhaib

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Actually I randomly ran into this solution yesterday by just poking around.  Thanks! I am going to make this as the solution! 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.