2025-06-10 6:14 AM
When trying to install STM32CubeMX 6.14.1 on Debian Linux, I get an error after the information about the collection of usage information:
[...]
You can stop the collection of your features usage statistics when you use the application at any time with effect for the future
or update your preferences via the menu
Help > User Preferences > General Settings
Press anything to continue
z
Analytics service enabled
SEVERE: Cannot invoke "java.lang.CharSequence.toString()" because "s" is null
[ Console installation FAILED! ]
WARNING: Cannot invoke "java.util.List.iterator()" because "this.files" is nullI start the installation script as
./SetupSTM32CubeMX-6.14.1in the unzipped folder of the CubeMX installer. Is this a known issue?
2025-06-10 6:18 AM
I'd like to add that the installer for version 6.12.1 worked without issues.
2025-06-10 9:25 AM
Hello @Lars Beiderbecke
First let me thank you for posting.
In fact according to the STM32CubeMX release note RN0094 Rev 76 section 1.2 Host PC system requirements, the Debian Linux destitution is not supported: Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 41
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-11 4:38 AM
Hello @Semer CHERNI,
Thanks for your quick reply.
While I don't really understand why a Java console program should be bound to specific Linux distribution versions, I'm happy to report that I get the very same error on Ubuntu 24.04.2 LTS (see attachment).
You owe me one hour for setting up that VM with Ubuntu.
Regards
Lars
2025-06-11 4:53 AM
2025-06-11 5:33 AM
> ... I get an error after the information about the collection of usage information: ...
I suspect you can safely ignore this error.
2025-06-11 7:54 AM
Hello @Lars Beiderbecke
I apologize for the misbehavior.
Let me further check the error message and come back to you asap.
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-12 4:12 AM
Thank you very much, I appreciate it!
2025-07-01 5:19 AM - edited 2025-07-01 5:33 AM
I just ran into this same issue today. Looking forward to see what can be done to get this to work.
I am running Ubuntu 22.04
2025-07-01 7:25 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.