STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

ST HAL I2C generating wrong address.

Posted on February 12, 2016 at 15:42 Hello, I've been working with ST HAL libraries for an STM32F030R8T6, using the NUCLEO board, and I'm having some problems with the I2C API. Probably it's a configuration issue but for the love of me, ...

0690X00000605MkQAI.png
jordi2 by Associate
  • 3258 Views
  • 3 replies
  • 1 kudos

STM32CubeMX GPIO Defined initial level after initialization

Posted on August 11, 2014 at 14:27To avoid glitches at the output, we initialize in the following order: 1. GPIOx clock enable 2. Set output registers to defined value 3. Perform initialization Now we would like to use STM32CubeMX. Is it possib...

0690X00000605fDQAQ.png
rm2399 by Associate III
  • 1188 Views
  • 2 replies
  • 0 kudos

Problem with CubeMX 4.5.0 with Linux

Posted on January 12, 2015 at 11:38Hello all. Bed path: java.io.FileNotFoundException: /home/krzysiek/STMicroelectronics/STM32Cube/STM32CubeMX/db/plugins/projectmanager\stm32tck.cfg (No such file or directory) at java.io.FileInputStream.open(Nativ...

giver3 by Associate II
  • 1282 Views
  • 2 replies
  • 0 kudos

LWIP process call frequency

Posted on February 04, 2016 at 11:25Hi all, Quite new in the development with LWIP, there is a question I have not found any answer so far; What is the minimum / maximuum frequency at which the main LWIP process function shall be called? I'm talking...

STM32CubeMX annoying behaviour

Posted on February 05, 2016 at 13:01Hi, I am using the current version (4.12.0) of STM32Cube. Every time I open a *.ioc file, it is immediately regarded as changed -- it's marked by a star in the window title and if I want to exit, I get a warning ...

zabel by Associate III
  • 836 Views
  • 0 replies
  • 0 kudos

STm32CubeMx Generated Code w/ RTOS for EWARM toolchain

Posted on January 28, 2016 at 22:18I used Stm32CubeMx with STM32Cube_FW_F0_V1.4.0 to generate my project on STM32F030CC with FreeRTOS and EWARM toolchain. In debug mode. I only have the generated code at this time. It first crashes on HAL_TIM_PWM_Co...

fsavaria by Associate II
  • 1031 Views
  • 1 replies
  • 0 kudos

STM32CubeMX not running

Posted on January 14, 2016 at 09:55My installation of STM32CubeMX is not working. I tried to reinstall the application but the Windows Control Panel -> Programs and Features Uninstall function does not work. I deleted the installation directory manu...

0690X00000604lBQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.