STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CubeMX F3 bug

Posted on January 23, 2016 at 15:27CubeMX: 4.12.0STM32Cube_FW: F3_V1.2.0MCU: Stm32F303VCT(stm32-f3-discovery)I configure OPAM4 to ''PGA not connected'', Non-inverting input is configured to PB11.Cube generates code:  hopamp4.Init.NonInvertingInput =...

elijah by Associate III
  • 1171 Views
  • 1 replies
  • 0 kudos

Strange output in STM32CubeMX Ver 4.12.0

Posted on January 22, 2016 at 22:09I recently upgrade CubeMX to version 4.12.0 and used it to generate code for a custom STM32F407VGT board. Everything seemed to work fine with previous versions, but not so much with the latest version. For example....

AN for runtime RAM/Stack usage of the STM32 application

Posted on January 21, 2016 at 17:20HI, Is there any Application Note for runtime stack and RAM utilization of the STM32 application .Any tool specific to Nucleo for evaluating the application?Is STM Studio meant for that?Rgds,R #!stm32-!cubemx #s...

darla14 by Senior
  • 1944 Views
  • 3 replies
  • 0 kudos

STM32CubeMX and F1 package v1.3

Posted on January 03, 2016 at 13:40I have STM32CubeMX v4.12, Check for Updates revealed STM32CubeF1 Release 1.3 After dondloadint , but Cube say: This Package version is not managed on this version of STM32CubeMX. Wher is probl�m?  I am talkingabout...

asrock70 by Associate II
  • 3708 Views
  • 6 replies
  • 0 kudos

Do I need both STM32CubeMX and STM32CubeF4?

Posted on May 13, 2014 at 04:41HelloI'm new with ST microcontrollers and reading the documentation I can see that there is STM32CubeMX and STM32CubeF4. I read also that STM32CubeMX contains the STM32CubeF4 or something like that.My question is; If S...

m4l490n by Senior
  • 3314 Views
  • 8 replies
  • 0 kudos

STM32CubeMX data model

Posted on December 01, 2015 at 12:41Hi, The STM32CubeMX data model is mentioned in the user manual UM1718, I'd like to use some more advanced custom code generation but am getting stopped by a lack of spec for the data model. Is the data model speci...

guy2399 by Associate
  • 1105 Views
  • 1 replies
  • 0 kudos

STM32CubeMX F3 Comparator & ADC -- AN4232

Posted on January 10, 2016 at 23:19I am reading through AN4232 on using the F3 comparator and it notes in section 2.3 that the comparator input is also an ADC channel.  I would like to use the channel for both, however I have not found a way in STM3...

STM32CubeMX does not allow setting CRC Polynomial

Posted on September 29, 2015 at 12:22I want to set the CR polynomial according to the most top table in http://users.ece.cmu.edu/~koopman/crc/index.html However STM32CubeMX does not allow to do it due to the following restrictions: ---- CRCPolynomia...

caco3 by Associate II
  • 1054 Views
  • 1 replies
  • 0 kudos

I2S code generated by STM32CubeMX for STM32F746 - no MCKO

Posted on December 12, 2015 at 19:37Hello,I'm using STM32CubeMX to generate a project for STM32F746VGT6.Everything works fine except I2S3, there is no clock output on MCKO pin (PC7) and the call of HAL_I2S_Transmit(...) generates a timeout error.The...

fmcarp by Associate
  • 2090 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.