STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CubeMX How to install expansions?

Posted on March 08, 2016 at 19:21Hi, I wanted to check out the WIFI Expansion for Cube MX. But I am failing at integrating it into CubeMX as I cannot find any information on how to integrate the downloadable expansions into CubeMX. Any help is appre...

hharte9 by Associate
  • 952 Views
  • 1 replies
  • 0 kudos

STM32CubeMX ftl template

Posted on March 08, 2016 at 11:08Hello guys, Can somebody share a list of all possible variables that I can use in FreeMarker templates inside of STM32CubeMX with me? I am working on a Makefile and .ld (because existing have not very nice license ;)...

STMCubeMX USE_FULL_ASSERT compile error when DAC enabled

Posted on March 03, 2016 at 14:28I have the STM32F303RE Nucleo evaluation board, and I've used CubeMX to configure & generate the HAL drivers. I've configured a DAC on one of the timers, and everything compiles/runs fine, except when I enabled ''USE...

yonkahlon by Associate II
  • 2039 Views
  • 2 replies
  • 0 kudos

Frustrated with UART&ADC dual mode

Posted on February 24, 2016 at 13:56 I am really got tired after so many attempt to use this hal drivers for ADC sampling in dual mode and send data over uart. For god sake plz help me. I did whatever user manuals said but still no output. ...

Reorganization of Cube headers

Posted on February 28, 2016 at 20:14It would be nice if you could move into a header the definition of GPIO_MODE, GPIO_MODE, ... GPIO_CR_CNF_ANALOG, GPIO_CR_MODE_INPUT, GPIO_CR_CNF_ANALOG, ...GPIO_CR_CNF_AF_OUTPUT_OD currently in stm32fNxx_hal_gpio....

CubeMX for STM32F746, unable to set a specific timer option

Posted on February 22, 2016 at 19:16Under ''slave mode'' the timer configuration of the TIMx_SMCR register: ''Combined Reset + trigger'' mode cannot be reached using the available menu items whereas ''reset mode'' or ''trigger mode'' are available.I...

jose luu by Associate III
  • 1279 Views
  • 2 replies
  • 0 kudos

CubeMX Mac?

Posted on February 26, 2016 at 02:46So eagle eye'd son pointed out that the publicity picture for CubeMX shows its logo sprawled across the face of Apple's MacBook Pro. And yet there are logos for Windows and Linux next to it.So, when is CubeMX goin...

UART Byte Loss

Posted on February 22, 2016 at 16:25I have two UARTs configured as follows (code generated by CubeMX).UART_HandleTypeDef huart2;UART_HandleTypeDef huart4;// Pins (Rx/Tx): PA3 / PA2 - Asynchronous (UART)void MX_USART2_UART_Init(void){ huart2.Instance...

UART Receive Interrupt on STM32f0 using CubeMX / Keil (how?)

Posted on February 16, 2016 at 09:02My tools: STM32f072rb (NUCLEO) MCP2200 uart to usb board STM32CubeMX (4.12.0) Keil uVision 5 (5.17) What I'm trying to do: Running a program in the main loop and reading UART transmission into a ring buffer. (as ...

Mnemocron by Associate III
  • 4097 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.