2016-01-28 1:18 PM
I used Stm32CubeMx with STM32Cube_FW_F0_V1.4.0 to generate my project on STM32F030CC with FreeRTOS and EWARM toolchain. In debug mode. I only have the generated code at this time. It first crashes on HAL_TIM_PWM_ConfigChannel() call. It seems to loop inside a strange memory area around 0x1FFFDA7C, or so says the debugger. Log window displays ''The stack pointer for CSTACK (currently 0x20000A78) is outside the stack range (0x200000B8 to 0x200004B8).
I decided to comment MX_TIM3_Init() in main.c, but to no avail. I ended up commenting all MX_() calls to keep it as simple as possible, now it crashes with the same behaviour, but on the line __DSB() inside vPortYield(). I then tried to stard without any other initialisation besides osKernelStart(), still won't work. Decided to see if any ISR are being called, and the answer is none, not even PendSV_Handler() nor SysTick_Handler(). Reset default clock settings or not, same problem. I now have an empty SystemInit() and a main() containing only osKernelStart(). I just won't work. Am I missing something here? #stm32f030cc-stm32cubemx-rtos2016-01-28 2:45 PM
Finally I switched debugger from J-Link Plus to ST-Link, problem solved. Symptom was really an unexpected system reset followed by unexpected boot load from system memory.
A lesson lived is a lesson learned.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.