STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

ioc switching

hi I'm using nucleo-h755 144 pin board, i have configured for the project, now I'm changing the mcu from stm32h745BITx 208 pin package. is there any option in stm32cubeide to import the configuration from one mcu to another mcu in cube ide without or...

STM32U545 CubeMX TrustZone Starter Config

Hello,I have an existing project and I'm attempting to retrofit it with TrustZone, starting with a new IOC file that will be the basis of the project which I will then retrofit my code into. I'm starting with a clean slate ioc file for the STM32U545C...

JTR by Associate
  • 1186 Views
  • 0 replies
  • 0 kudos

Using DMA with UART Idle Timeout on STM32G4

Hi Team,I'm currently transitioning from using UART interrupt with timeout to DMA-based reception on an STM32G4 controller. I’d like to implement a similar behavior where I can detect the end of a UART message using idle line detection while receivin...

Failed in update the firmware package for STM32H5

I download the latest firmware package "stm32cubeh5-v1-5-0.zip" for STM32H5, from ST's website. I followed following instructions to install it via STM32CubeMX:Open STM32CubeMX.  Go to Help > Manage embedded software packages.  Choose the desired STM...

WenLiu_0-1752236346137.png
Wen-Liu by Associate
  • 1150 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMX CAD export fails

I am using STM32CubeMX Version 6.13.0 and targeting the STM32H743BIT6.The CAD export option fails with the error: "Download interruption: CAD download fails due to AxiosError: Request failed with status code 500".I first experienced this with an olde...

STM32CubeMX CAD Download Error.png
MPamenter by Associate II
  • 2817 Views
  • 5 replies
  • 1 kudos

Resolved! STM32G030F6P ADC Frequency in STM32CubeMX

I was checking maximum frequencies of some MCUs and noticed i can pick ADC frequency in CubeMX clock configuration up to 80MHz for TSSOP-20 STM32G030. Its maximum frequency is 64MHz.Datasheet states it can deliver maximum 2Msps on 12 bit but with its...

MKanc.1 by Associate III
  • 2048 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.