STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! CubeMX creates broken SystemClock_Config()

Posted on November 04, 2016 at 13:42 In STM32Cube MX 4.17 I have set up an empty STM32L476 Nucleo project with and created code for the Low-Layer API. The parameters were: LL_PWR_REGU_VOLTAGE_SCALE2LL_RCC_MSIRANGE_8 The function System...

STM32CubeMX 4.19.0 Code generation issue

Posted on February 26, 2017 at 19:34Hi.I have noticed some problems when generating code using STM32CubeMX 4.19.0. I included the zipped project in the attachments. In the Src/main.c file it generates the declaration of the FSMC init functionstatic ...

petoknm by Associate II
  • 2631 Views
  • 4 replies
  • 0 kudos

Extremely slow CubeMX in Clock View on OSX.

Posted on December 06, 2016 at 21:19Cube slows down the point when it is pretty much very hard to use. Sometimes clock resolver ends up in an continous loop which leads nowhere. Also on chips with more pins like BGA packages Cube slows down noticeab...

ChrisH by Associate III
  • 4173 Views
  • 10 replies
  • 0 kudos

USB-FS MSC Slow Writing Speed

Posted on March 05, 2017 at 20:12Hi,I'm using STM32F4 as a USB Host for writing data to a mass storage (flash drive) in FS mode using CubeMX. As we know USB-FS nominal speed is 12Mbit/s and I set this speed in CubeMX for my application. However, the...

Resolved! [BUG]STM32CubeMX - Project loading

Posted on January 27, 2017 at 10:38I use STM32CubeMX ver. 4.19.0.I've configured DMA channel for I2S peripheral and saved the project. But when I try to open it again I get this warning:The project is attached.#bug #i2s #stm32cubemx #dma

0690X000006069mQAA.png
Eugene S. by Associate III
  • 5020 Views
  • 10 replies
  • 0 kudos

CubeMX, STM32L476, USART Parity problem

Posted on February 15, 2017 at 12:22Hello everybody,I encountered the following problem when generating code from CubeMX for the USART peripheral of a STM32L476QEIx:SETUP: STM32CubeMX 4.19.0CubeL4 Version 1.6.0CPU STM32L476QEIxPROBLEM: USART1 is c...

STM32CubeMX generates broken SW4STM32 code

Posted on December 31, 2016 at 08:52 Hi, I've created a very simple project in STM32CubeMX for the F3DISCOVERY board. The only things I changed from the default are enabling MCO, and setting the PLL multiplier to When I import the code into S...

jeremyh by Associate II
  • 5612 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.