STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1759 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX 4.18.0 error in .cproject on OSX

Posted on December 11, 2016 at 23:47Since the last update to CubeMX, new projects created for SW4STM32 on OSX are not compiling anymore. The project settings for C symbols are missing quotes:__weak=__attribute__((weak)) instead of __weak='__attribut...

CubeMX ''user code'' request

Posted on March 31, 2017 at 13:35Hi, I would like to sugest an insertion of 'user code' entry inthe MX_***_Init() functions between the Peripheral init and its NVIC config, like:...... GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING; GPIO_InitStruct.P...

STM32 VCP plug and play

Posted on April 07, 2017 at 08:05Hello,im using the STM32F407 DIS with CubeMX to generate a USB CDC device.All works fine but if i unplug the STM32f407 and then plug in, Windows 10 didnt detect the driver(just unknown USB-Device)i have to reset the ...

Ethernet-TCPip Nucleo F429ZIT6

Posted on April 06, 2017 at 13:14Hi,I use STM32CubeMX to generate the configuration of LWip on my card (nucleo F429ZIT6). Once my card program, I address a fixed IP address but I can't see my card on the local networks.The code generated is :int mai...

STM32-MAT Simulink problems

Posted on March 16, 2017 at 13:08I am trying to get the STM32-MAT package to work with Simulink to do some test on a stm32f4discovery board and I am running into multiple issues.1. A simple Simulink setup for a normal build:When building this simple...

0690X00000606a4QAA.png 0690X00000606aOQAQ.png 0690X00000606DdQAI.png 0690X00000606XzQAI.png

Touch Sensing with CubeMX and stm32l152-discovery

Posted on September 16, 2016 at 22:59I'm really struggling to get Touch Sensing working on the stm32L152 RCT6 discovery board. I'm trying to use it with CubeMX and understand that there is a particular procedure to use the Touch lib with CubeMX. Cou...

Cube MX Timer init Error on STM32F050R8

Posted on April 04, 2017 at 16:29Using the attached cube project TestSTM32F051R8_TimError.iocWhen I generate the source codes the CubeMx version  4.20.0 produces the following initialization code for the timers (I used only TIM1 and TIM3) but the er...

STM32F4 Memory Card Interface Issue

Posted on February 22, 2017 at 14:43Hello. I am trying to integrate SD Card (Transcend 4GB) with STM32F407 Disc board. I had followed all previous discussion & made corrections yet i am getting Error. I have attached my clock configuration, Pin diag...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.