2016-12-30 11:52 PM
Hi,
I've created a very simple project in STM32CubeMX for the F3DISCOVERY board. The only things I changed from the default are enabling MCO, and setting the PLL multiplier to When I import the code into SW4STM32 and press build, I get the following error:
17:41:40 **** Build of configuration Debug for project test_64mhz ****
make all
Building file: ../Src/main.c
Invoking: MCU GCC Compiler
/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Debug
arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F303xC -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc/Legacy' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Device/ST/STM32F3xx/Include' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Include' -Os -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF'Src/main.d' -MT'Src/main.o' -o 'Src/main.o' '../Src/main.c'
/bin/sh: -c: line 0: syntax error near unexpected token `('
/bin/sh: -c: line 0: `arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F303xC -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/STM32F3xx_HAL_Driver/Inc/Legacy' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Device/ST/STM32F3xx/Include' -I'/Users/jeremy/stm32_test/rcc_64mhz/test_64mhz/Drivers/CMSIS/Include' -Os -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF'Src/main.d' -MT'Src/main.o' -o 'Src/main.o' '../Src/main.c''
make: *** [Src/main.o] Error 2
17:41:40 Build Finished (took 94ms)�?�?�?�?�?�?�?�?�?�?�?
My operating system is OSX Yosemite, and both SW4STM32 and STM32CubeMX are updated to the latest versions.
Thanks,
Jeremy
#stm32cubemx #sw4stm322016-12-31 12:00 AM
Posted on December 31, 2016 at 09:00
This has been reported to ST and the people at AC6 that take care of SW4STM
<LINK NO LONGER ACTIVE>
https://community.st.com/0D50X00009Xke6gSAB
Andrei
2017-01-02 2:06 AM
Posted on January 02, 2017 at 11:06
Hi
Herbert.Jeremy
,
The issue has been reported to our MXteam for checking.
Sorry for the inconvenience may bring.
-Nesrine-
We are looking for your wishes about our STM32 products,ecosystem and community:
<LINK NO LONGER ACTIVE>
2017-01-10 7:21 AM
2017-01-16 4:53 AM
Dear Users,
This issue (encountered on MAC and Linux OS only) will be fixed with STM32CubeMX 4.19 next release.
Best regards
2017-01-18 8:20 AM
Dear User,
Indeed, this is a regression introduced by Ac6 into the v1.13.
A fix is already under implementation. As temporary solutions, the 2 following workarounds are proposed :
1 – Workaround #1:
In the following post, the user reverted the installation (back to V1.12) and it solved the issue.
http://www.openstm32.org/tiki-view_forum_thread.php?forumId=7&comments_parentId=4390#threadId7
How to revert : Help menu >> Installation Details >> Installation History tab >> Select the V1.12 configuration >> Revert
2 – Workaround #2:
Navigate to <SW4STM32_INSTALL>/plugins/fr.ac6.mcu.externaltools.arm-none.win32/tools/make;
Make a backup of the folder;
Remove the files:
echo.exe
msys-1.0.dll
msys-iconv-2.dll
make/msys-intl-8.dll
msys-regex-1.dll
msys-termcap-0.dll
sh.exe
Sorry for inconveniences.
Best regards,
Alain
2017-01-18 2:23 PM
Good evening ,
I've a similar issue on my IDE (eclipse), I use STM32CubeMX (the lastet, updrade done 18 January 2017).
During compilation I've this message on eclipse
23:17:50 **** Incremental Build of configuration Debug for project Horloge_CC ****
make all Building file: ../Src/crc.cInvoking: MCU GCC Compiler/home/joachim/workspace/Horloge_CC/Debugarm-none-eabi-gcc -mcpu=cortex-m7 -mthumb -mfloat-abi=hard -mfpu=fpv5-sp-d16 -D__weak=__attribute__((weak)) -D__packed=__attribute__((__packed__)) -DUSE_HAL_DRIVER -DSTM32F746xx -I'/home/joachim/workspace/Horloge_CC/Inc' -I../Drivers -I../Middlewares -I../Drivers/STM32F7xx_HAL_Driver -I../Middlewares/USB_Device_Library -O0 -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF'Src/crc.d' -MT'Src/crc.o' -o 'Src/crc.o' '../Src/crc.c'/bin/sh: 1: Syntax error: '(' unexpectedSrc/subdir.mk:66: recipe for target 'Src/crc.o' failedmake: *** [Src/crc.o] Error 223:17:50 Build Finished (took 63ms)
I've done a similar project without cube with no problem. I use linux Debian (3.16.0-4-amd64 #1 SMP Debian 3.16.36-1+deb8u2 (2016-10-19) x86_64 GNU/Linux)
Who can help me ?
Regards
Joachim
2017-01-18 3:51 PM
select your eclipse project in Project Explorer, then right click
choose 'Properties'
choose C/C++ Build
choose Symbols
change __weak=__attribute__((weak)) to __weak='__attribute__((weak))'
change __packed=__attribute__((__packed__)) to __packed='__attribute__((__packed__))'
2017-01-27 3:25 AM
Hello All,
Eclipse plugins has been patched.
You can check for updates, and upgrade to version 1.13.1.201701200843
Kind regards
Sirma
2017-02-20 2:56 AM
Hello,
the problem is present again in 'OpenSTM32 IDE 1.13.1.201701261206', running on Windows 10 64bit
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.