STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Bug: CubeMX 4.25 path changes in Makefile

Posted on March 20, 2018 at 03:21After upgrading to 4.25 and regenerating the project, I went through a diff of all the changes in generated code since the previous version. The majority were whitespace and comment changes which were fine.But I did ...

0690X0000060AAZQA2.png 0690X0000060AAjQAM.png

STM32F4Discovery, CubeMX, and default RCC

Posted on March 08, 2018 at 00:01Creating a project using version 4.24 of CubeMX for the STM32F4Discovery board, I select 'yes' to 'Initialize all peripherals with their default Mode.'The RCC block selects 'Crystal/Ceramic Resonator' for the LSE.  H...

Resolved! STM32F446 - why PB12 conflicts with USB PHY?

Posted on March 07, 2018 at 00:16Why CubeMX 4.24 says that PB12 conflicts with USB_OTG_HS when external HS PHY is not is use?The MCU is F446ZCT, its USB HS core is in FS, host only mode, Activate_SOF and Activate_VBUS unchecked.PB12 can have two alt...

0690X00000609y0QAA.png
Pavel A. by Super User
  • 2629 Views
  • 7 replies
  • 0 kudos

Commercial usage of code generated by STM32CubeMX

Posted on March 07, 2018 at 13:49Hello ST community,Our customer requested a software development for his device based on a ST microcontroller. After the development process ends he wants to have the source code what is a common condition for a serv...

CubeMX makefile errors

Posted on January 19, 2018 at 16:12The makefile output feature of CMX is really great but as others have said here it has  bugs that make it somewhat problematic, and it appears that ST are not taking it too seriously.I am trying to use CMX with Vis...

Frank CA by Associate III
  • 3193 Views
  • 4 replies
  • 0 kudos

Timer config in CubeMX

Posted on February 14, 2018 at 14:43Would be very helpful if the Cube automatically showed the clock frequency for timers in Configuration view.Otherwise I have to dig out of the RM which bus corresponds to specific timer - AHB1 or AHB2, then open t...

Pavel A. by Super User
  • 1666 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeMX USB CDC defaults do not compile

Posted on October 04, 2017 at 11:52Hi,Currently the defaults set for STM32F042 in STM32CubeMX v4.22.1, FW 1.9.0 for USB CDC will not compile after generation.This is because the USB CDC Rx and Tx Buffers are set to 2048B each by default, which is to...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.