2017-08-06 10:22 AM
Hello!!
I post an .IOC file that produces initialization code for Keil v5.
This file produced with 4.22 version of CubeMX and uses the latest firmaware for L1 family.
At module, gpio.c and especialy inside called function LL_SYSCFG_SetEXTISource(LL_AHB1_GRP1_PERIPH_GPIOA, LL_SYSCFG_EXTI_LINE0); , the first parameter,
LL_AHB1_GRP1_PERIPH_GPIOA
is not correct.Inside the module stm32l1xx_ll_system.h, contained the right parameters must put.
This parameter has value 0x01, but the correct LL_SYSCFG_EXTI_PORTA has value 0x00.
This cause problem to set the correct source of EXTI interrupts.
#ll #stm32cubemxSolved! Go to Solution.
2018-03-05 5:36 AM
Hi
FORTOUNAS.EVANGELOS
,
This issue is fixed in the current CubeMX release (4.24).
Please upgrade your cubeMX release if not already done.
BR. Jeanne
2017-08-24 5:55 AM
Hi
FORTOUNAS.EVANGELOS
,I confirm this issue from my side and I would like to thank you for highlighting it.
It is reported internally so that a fix can be planned for coming releases of CubeMX.
Best Regards,
Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-03-05 5:36 AM
Hi
FORTOUNAS.EVANGELOS
,
This issue is fixed in the current CubeMX release (4.24).
Please upgrade your cubeMX release if not already done.
BR. Jeanne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.