STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

ST67W6X_CLI lockup

Issue: ST67W6X_CLI lockup Test Setup:Use the ST67W6X_CLI example provided with the x-cube-st67w61-v1.0.0 software package.Send wifi_sta_connect command to connect.Send several ping commands to verify connection.Keep the connation active.Wait for 5 to...

CMake Build Issue with STM32H563ZI

Hi ST team, Been trying to build a bare bones MX generated project for the STM32H563ZI using CMake, for both TrustZone and non-TrustZone Projects. Had the same issue on both Ubuntu22.04 and Ubuntu24.04, and am unable to compile any of these projects....

lachjet by Associate II
  • 2288 Views
  • 8 replies
  • 0 kudos

Resolved! Creating STM32N6 ioc project for hexaSPI and octoSPI.

Hello,While creating a project for STM32N6 I can’t find the option for hexaspi or octospi for STM32N657B0HxQ . Is there any particular option I have to enable?I am trying to generate the ioc similar to STM32N6570-DK board .I am on 6.15.0 STM32CubeMX....

darla14_0-1758621776963.png
darla14 by Senior
  • 1244 Views
  • 5 replies
  • 2 kudos

Resolved! STM32F070 APB1 clock can't be configured with HSI clock

Hi,APB1 clock can't be enabled if HSI clock is chosen. It says that the driven clock must be 10M<=x<48M, so, without using the PLL it's impossible to get the 10MHz. Things get worse when I try to feed the PLL from the HSI: it says that the PLL should...

Captura de pantalla de 2025-09-20 00-08-43.png 20250919_235605_1758347808903.jpg Captura de pantalla de 2025-09-20 00-24-25.png
XR.1 by Senior
  • 932 Views
  • 2 replies
  • 1 kudos

Resolved! STM32 Cube MX STM32U535 ADC Error

Hi,Running STM32MX Tool 6.15.0 On Windows 10.Started a project for a STM32U535CCTx.I've enabled ADC and configured channel IN8. The software thinks this is connected to PA4, but the datasheet says it is connected to PA3. See screen caps below. Regard...

jminack_0-1757905070998.png jminack_1-1757905125016.png
jminack by Associate II
  • 1101 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.